I'm trying to use the S32K148 MCU.
The available combinations are
Case 1. S32 Design Studio 3.4 + S32SDK S32K1xx RTM 4.0.3,
Case 2. S32 Design Studio 3.5 + S32SDK S32K1xx RTM 4.0.1.
Can't I use it like the following combination ?
Case 3. S32 Design Studio 3.5 + S32SDK S32K1xx RTM 4.0.3.
(I tried, but I couldn't.)
If not, which of Case 1 and Case 2 above is not a problem to use?
Thanks
Cheolhyeon Cho