What choice should I make using S32 Design Studio for S32 Platform version for S32K148 MCU ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What choice should I make using S32 Design Studio for S32 Platform version for S32K148 MCU ?

Jump to solution
1,372 Views
toipaz
Contributor III

I'm trying to use the S32K148 MCU.

The available combinations are

Case 1. S32 Design Studio 3.4 + S32SDK S32K1xx RTM 4.0.3,
Case 2. S32 Design Studio 3.5 + S32SDK S32K1xx RTM 4.0.1.

Can't I use it like the following combination ?

Case 3. S32 Design Studio 3.5 + S32SDK S32K1xx RTM 4.0.3.

(I tried, but I couldn't.)

If not, which of Case 1 and Case 2 above is not a problem to use?

Thanks

Cheolhyeon Cho

Labels (1)
0 Kudos
Reply
1 Solution
1,362 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Cheolhyeon Cho,

According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version. So please select: Case 1. S32 Design Studio 3.4 + S32SDK S32K1xx RTM 4.0.3


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,363 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Cheolhyeon Cho,

According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version. So please select: Case 1. S32 Design Studio 3.4 + S32SDK S32K1xx RTM 4.0.3


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,355 Views
toipaz
Contributor III
Robin
Thanks.
0 Kudos
Reply