What choice should I make using S32 Design Studio for S32 Platform version for S32K148 MCU ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What choice should I make using S32 Design Studio for S32 Platform version for S32K148 MCU ?

跳至解决方案
1,375 次查看
toipaz
Contributor III

I'm trying to use the S32K148 MCU.

The available combinations are

Case 1. S32 Design Studio 3.4 + S32SDK S32K1xx RTM 4.0.3,
Case 2. S32 Design Studio 3.5 + S32SDK S32K1xx RTM 4.0.1.

Can't I use it like the following combination ?

Case 3. S32 Design Studio 3.5 + S32SDK S32K1xx RTM 4.0.3.

(I tried, but I couldn't.)

If not, which of Case 1 and Case 2 above is not a problem to use?

Thanks

Cheolhyeon Cho

标签 (1)
0 项奖励
回复
1 解答
1,365 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Cheolhyeon Cho,

According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version. So please select: Case 1. S32 Design Studio 3.4 + S32SDK S32K1xx RTM 4.0.3


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,366 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Cheolhyeon Cho,

According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version. So please select: Case 1. S32 Design Studio 3.4 + S32SDK S32K1xx RTM 4.0.3


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,358 次查看
toipaz
Contributor III
Robin
Thanks.
0 项奖励
回复