Unable to open example projects S32 after sdk update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to open example projects S32 after sdk update

ソリューションへジャンプ
2,922件の閲覧回数
johannesmaier
Contributor I

Hi,

since i´ve installed the sdk version 0.86, i can´t open example projects anymore.

At first i tried the usual way "File->New->S32DS Project from Example", but nothing happens.

After that i tried "Open Projects from File Browser" and inserted the sdk 0.86 installation path. But no project opens.

With version 0.84 and 0.85 it worked.

Using:

S32 Design Studio for ARM

Version 2.0

Build id: 170810

Hoping for help

Johannes

ラベル(1)
1 解決策
2,677件の閲覧回数
johannesmaier
Contributor I

Hi Jiri,

thank you for your quick answer.

Re-installing SDK didn´t work, but i think i found the problem now.

I completely re-installed Design Studio(+sdk) with the PC administrator and it seems that i didn´t have enough rights as a normal user.

After installation the admin tried to open the examples and it worked, then i tried the same with my user account but it didn´t work.

the admin changed rights for s32 folder, so it works now.

Johannes

元の投稿で解決策を見る

2 返答(返信)
2,677件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Johannes, 

you can try to uninstall the update and install it again. For me is SDK v0.8.6 working okay. For uninstall click on Help -> Installation details and find SDK installation: 

pastedImage_1.png

Hope it helps. 

Jiri 

0 件の賞賛
返信
2,678件の閲覧回数
johannesmaier
Contributor I

Hi Jiri,

thank you for your quick answer.

Re-installing SDK didn´t work, but i think i found the problem now.

I completely re-installed Design Studio(+sdk) with the PC administrator and it seems that i didn´t have enough rights as a normal user.

After installation the admin tried to open the examples and it worked, then i tried the same with my user account but it didn´t work.

the admin changed rights for s32 folder, so it works now.

Johannes