Unable to mount root fs on unknown-block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to mount root fs on unknown-block

Jump to solution
2,032 Views
aiweixin
Contributor IV

I have created a bootable SD Card for the S32R45 EVB by writing the fsl-image-auto-s32r45evb.sdcard image file(use Win32DiskImager).

aiweixin_0-1669887424962.png

aiweixin_1-1669887440105.png

Insert the SD card into the S32R45 EVB SD slot, and power-on the EVB. It seems unnormal, points out “unable to mount root fs on unknown-block”.

How can I do to solve it?

 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,006 Views
alejandrolozan1
NXP Employee
NXP Employee

Hello, 

 

It seems the second partition EXT3 where the rootfs resides, was not written correctly. 

Could you insert the SD card in a Linux host and make sure you get 2 partitions in the SD card?

The first one must be a FAT32 and the second one Ext3/Ext4. 

 

Saludos,

Alejandro

View solution in original post

0 Kudos
Reply
2 Replies
2,007 Views
alejandrolozan1
NXP Employee
NXP Employee

Hello, 

 

It seems the second partition EXT3 where the rootfs resides, was not written correctly. 

Could you insert the SD card in a Linux host and make sure you get 2 partitions in the SD card?

The first one must be a FAT32 and the second one Ext3/Ext4. 

 

Saludos,

Alejandro

0 Kudos
Reply
2,001 Views
aiweixin
Contributor IV

Dear,

    I have replaced another SD card, it seems working normally.

    Thank you!

0 Kudos
Reply