The execution problem on S32V234 EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The execution problem on S32V234 EVB

1,639 次查看
ccliao
Contributor I

I have installed【VisionSDK_S32V2_RTM_1_3_0】 and updated【S32V2-AIRUNNER-LINUX-EAR-0.8.0_AIR02】 in my machine. I have compiled successfully the sample of air_object_detection_st, as shown in the following picture,

compile.PNG

When I put the .elf file on the S32V234 EVB and execute it, the error messages are as follows,

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

I found the problem is that execute "net_mssd->Run()", attached please find the following picture,

pastedImage_5.png

How could I fix this problem?

Thank you.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,400 次查看
leyi_bjtu
Contributor I

Have you solved the problem yet? I got some problems similar to you.I have installed "VisionSDK_S32V2_RTM_1_5_1" and "S32V2-eIQAuto01_RTM_2_0_0". When I run the demo, I got following result:

airunner.jpg 

0 项奖励
回复