Board: S32R274 with PE micro multilink debugger
Program: RSDK OFFLINE demo
Make: Error 1
Ld error: rsdk_offline_example_sa_gcc_s32R274_z4_debug.elf.section ‘.data_noncache’ will not fit in ‘c0_sram’
Ld error: region ‘c0_sram’ overflowed by 62720 bytes
Everything runs smoothly, debugger printf shows on PC.Only file IO is not working. Every time I add TFTP_CLIENT_EN I get the above error and am unable to build properly.
What is the cause of this error? I am using the given code from the demo only, and I do not know where there could be a mistake.I would really appreciate some assistance regarding this topic.
Hello,
The offline example doesn't work with PE Debugger out of the box. A better example for this is the 1RF_4Antennas_demo.
Of course the customer can modify the offline example to work with the debugger but certain adjustments need to be done because PE micro does not have FILE-IO so the tftp configuration cannot be read.
Best regards,
Peter