System frequency of S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

System frequency of S32K144

956件の閲覧回数
zhangchun
Contributor III

hello

I am currently optimizing a piece of code and need to increase the system frequency. What is the maximum system frequency that Love can use when S32K144 is running stably? How should I configure it? Please provide a configuration example using S32DS,

thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

937件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@zhangchun

I see you already set the max clock for HSRUN mode and that is already the max.

Senlent_0-1687328346974.png

Have you try set the device run in HSRUN mode?  If yes, there is nothing I can do for you.

0 件の賞賛
返信

948件の閲覧回数
zhangchun
Contributor III

Currently using 80MHz, but still unable to meet the requirements

zhangchun_0-1687315284523.png

 

 

0 件の賞賛
返信