Serial Interface doesn't work - S32K3x4-Q172

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Serial Interface doesn't work - S32K3x4-Q172

858 次查看
MVR
Contributor III

Hello,

I'm using:

S32K3x4-Q172 and S32K3 RTD AUTOSAR 4.4 2.0.1 D2207. 

I'm testing the serial interface (LPUART6) but it doesn't work. I can see the signal in pin 2 of J44 when I send data in TX line but on PC I can't see data arriving on serial software. The baudrate is ok and the port of board appear correctly on device manager. Also I check the power supply of NTS0102GD and everything is ok.

MVR_0-1663358975971.png

It must be problem with MK26FN2M0VMI18?

Thanks

标签 (1)
0 项奖励
回复
3 回复数

845 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi MVR,

Seems that the problem is related the OpenSDA firmware of K26. Please refer to the discussion in: request K26's OpenSDA firmware on the S32K3X4EVB-Q172

Maybe PEMicro will send you the latest K26 Embedded Multilink firmware with full virtual serial port support.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

822 次查看
MVR
Contributor III

Hello Robin,

I talked with pemicro team and updated the FW.

But it doesn't work yet, I can see the signal as I said on TX line but on serial software it doesn't appear... 

Do you have any idea how can I fix it?

 

0 项奖励
回复

812 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Did you install the Virtual COM Port Drivers ?

 

 

0 项奖励
回复