SJA1110 L2 Lookup Table Trap Flag

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1110 L2 Lookup Table Trap Flag

1,023 Views
Stefan5
Contributor I

Hello,

I'm using the S32 Design Studio and config two L2 Lookup Tables for Switch 1 and Switch 2. The first one is working and my traffic forwarded to Port 0, which is the Buffer, but I can't transfer data from the other direction. "Host unreachable"

I use the two RJ45 Ports to connect with each other.

First L2 Lookup Table

Stefan5_0-1650462399044.png

 

Second L2 Lookup Table

Stefan5_1-1650462428007.png

Am I right that on the second L2 Lookup Table Port 2 is the RJ45 connector and Port 0 is the ENET Buffer, because the config using cascading?

Thank you and greetings

Stefan

 

Labels (1)
0 Kudos
Reply
0 Replies