Hello,
As to the problem I met: Errors in official example
I reinstall the S32DS. This time I use the latest version "S32DS_ARM_Win32_v2.2.exe".
After installation, I have not installed any patches, like "update11".
But when I try to create a new project, I cannot choose any SDKs. Please see the picture below:
I think there is already a SDK installed in my S32DS:
Can anyone help me, why can't I choose "RTM SDK 3.0.0" in my project?
Thanks!
Lu
解決済! 解決策の投稿を見る。
 
					
				
		
 raresvasile
		
			raresvasile
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Lu,
The sequence:
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE); 
can be replaced with:
CLOCK_DRV_Init(&clockMan1_InitConfig0);
Best regards,
Rares
 
					
				
		
 jiri_kral
		
			jiri_kral
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
you probably chose Standard S32DS toolchain for ARM when you created new project.. Please select ARM Bare-Metal 32-bit Target Binary toolchain.
Jiri
Thanks Jiri.
Yes, you're right.
When I choose the "ARM Bare-Metal 32-bit Target Binary toolchain", I can see the SDK 3.0.0.
But In this way, I will encounter the previous problem again:What are the differences between different toolchains?
When the "ARM Bare-Metal 32-bit Target Binary Toolchain" is used,then I cannot find the "CLOCK_SYS_Init" function in the "clock_manager".
Do you know why?
Thank you again!
Lu
 
					
				
		
 jiri_kral
		
			jiri_kral
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
this is very interesting question - I didn't realize yet that the function set is different. More strange thing is, that in Examples is used CLOCK_SYS_Init(...) but clock manager component offers only CLOCK_DRV_Init(...). To be honest - have no idea why is this component acting this way. So, I'll move your thread into S32 SDK community space. Someone from SDK team will answer your question.
Jiri
Ok thank you!
I wait for your message.
Lu
 
					
				
		
 raresvasile
		
			raresvasile
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
The CLOCK_SYS_* API was deprecated, this is why it was removed from the list.
It can still be used, but we recommend using CLOCK_DRV_* functions.
Thank you,
Rares
Hi, Rares
Thanks for your answer.
But I found that most of the official examples use these two functions to initialize:
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);
Can you provide some new examples, which use "CLOCK_DRV_* functions" ?
Give me some guidance.
Thank you!
Lu
 
					
				
		
 raresvasile
		
			raresvasile
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Lu,
The sequence:
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE); 
can be replaced with:
CLOCK_DRV_Init(&clockMan1_InitConfig0);
Best regards,
Rares
 
					
				
		
I would recommend following:
1) Update SDK examples to match 3.0.2 command set. Presently the examples utilize the deprecated functions, but the SDK does not include those.
2) S32DS should really make it clear that 3.0.2 is the version being used. If you install S32DS for ARM 2.2, it comes with 3.0.2, but as in the screenshots above the user only sees 3.0.0 listed. This is super confusing.