SDK 32K - ISO 26262 - certification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK 32K - ISO 26262 - certification

1,153件の閲覧回数
bavarian_simon
Contributor I

Dear all,

at the moment, our customer is using

NXP S32K148 with the SDK: NXP RTM 3.0.2,

NXP S32K116 with the SDK: NXP 1.8.7 EAR

and NXP S32K144 with the SDK: NXP RTM 3.0.2.

As far as I know, all three SDKs are not compliant with ASIL B of ISO 26262.

Are there any alternatives, which fulfill this requriement and how much effort is needed to convert?

Thanks for any help

Simon

ラベル(1)
0 件の賞賛
返信
1 返信

1,140件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have replied to your internal case.

Have a great day.