S32k144 flash time very high

cancel
Showing results for 
Search instead for 
Did you mean: 

S32k144 flash time very high

Jump to solution
589 Views
Raphael2
Contributor III

Hello,

Under: S32 Design Studio for ARM Version 2018.R1

I followed the guide to simply toggle between the green and red LED.

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-the-Blinking-LED-example-...

After building I debugged it, but the process takes between 3-4 minutes. I tried to build and debug it for RAM and flash but no difference. In debug process it gets stuck at around 50-60%. There are no errors and the program works after debug.

 

Under: MATLAB R2019b

I tried to flash the 'hello world' example in Simulink with the embedded coder and here Simulink and Matlab get stuck in the Building process and don't react anymore. After over 20 minutes I closed the process.

Praemas_0-1626345097105.png

I don't know if these warnings are of any importance.

Praemas_1-1626345149816.png

This are the last lines in Diagnostic Viewer.

I should add, that I had another s32k144 EVB and with this board the flashing process had no difficulties.

Because both programs take longer with this board I guess there is something wrong with the code transfer to the board.

How can I fix this?

 

Best regards

Labels (1)
0 Kudos
1 Solution
556 Views
Raphael2
Contributor III

Hello again,

thank you @Robin_Shen , but actually this wasn't the problem.

The company laptop runs an encryption for the usb port by default which I had to disable.

Now both flashing variants I tried work as usual.

Best regards

Raphael

View solution in original post

0 Kudos
3 Replies
573 Views
Raphael2
Contributor III

I need to add that I tried it with a new s32k144 EVB and still got the same problem

0 Kudos
564 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Raphael2,

Please refer: MultLink connect target with a long time
Hope it helps.

If still not work, please try to delete the workspace and create a new workspace.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
557 Views
Raphael2
Contributor III

Hello again,

thank you @Robin_Shen , but actually this wasn't the problem.

The company laptop runs an encryption for the usb port by default which I had to disable.

Now both flashing variants I tried work as usual.

Best regards

Raphael

0 Kudos