S32k SDK build Project Name change

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32k SDK build Project Name change

1,796 次查看
abhijithshankaren
Contributor I

 

HI,
  In s32 SDK the build project creates a .elf, with projectname.elf as default.

But is there any way, without changing the projects name
I want to have the .elf name, of my choice ? I do not want to rename pressing F2, instead when I give build project it should generate the .hex/.ellf  with name of my choice. Is there a way to do this ?
 

Regards
Abhijith Shankar

标签 (1)
0 项奖励
回复
1 回复

1,781 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Abhijith Shankar,

You can change the name of elf file in Build Artifact tab:

Artifact name.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复