S32V234 Vision SDK APEX Face Detection Demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32V234 Vision SDK APEX Face Detection Demo

1,253 Views
naomi_nomura
Contributor II

Dear NXP Technical team,

 

I bought the S32V234-EVB2 (Full EVB) and tried Vision SDK demo as a first try.

Because I have not had enough knowledge about S32V and Vision SDK demo, could you let me ask about the simple algorithm of following demonstration?

(Please refer VisionSDK_S32V2_RTM_1_3_0_UserGuide.pdf ?)

 

  1. apps/pex_isp_face_detection_cv

  When the faces are detected, the boundering box appear with the several colors (blue, light blue, green, yellow and red)

What does these color mean?

As long as I tested, the blue, light blue and green boxes appear well.

 

  1. apexcv_camdisp

The descriptin of this demo is mentioned as blow in the “Description” of the Vision SDK user Guide.

“Application with camera input and display, using APEX-CV functions to invert a color channel depending on the intensity in the green channel.”

Could you give me more explanation about the sentence “to invert a color channel depending on the intensity in the green channel.”?

I’m not clear why the color changes according to the object.

 

Best Regards,

Naomi Nomura

Labels (1)
0 Kudos
Reply
1 Reply

1,106 Views
bpe
NXP Employee
NXP Employee

My apologies for not updating this sooner, please be aware that all
support to S32V234 APEX, ISP and VSDK is done only via tickets.
I will contact you by e-Mail to provide answers you asked here, for
future requests about the products/features mentioned above,

please use only tickets.

Regards,

Platon

0 Kudos
Reply