S32R458 Premium Radar SDK Evaluation Package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R458 Premium Radar SDK Evaluation Package

2,179件の閲覧回数
CSBoy
Contributor II

Hi,

I used the installation package  is [S32r45_premium_Radar_SDK_evaluation_Package_0_8_0_220519.exe]

After installation, the build and project directories could not be found in each module of the PRSDK Algorithm. For example [TFDT Algorithm]

CSBoy_0-1659323918701.png

But, in the PRSDK_User_Manual file,Mention that users can compile and import projects,

CSBoy_1-1659324212114.pngCSBoy_2-1659324301483.png

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,168件の閲覧回数
HaoRen
NXP Employee
NXP Employee

Hi,

I have tested several recently updated installation packages, but there is no installation problem you mentioned. Please confirm whether you added the license file during installation, or download the latest package to test again.

nxf47389_0-1659405263357.png

 

nxf47389_1-1659405279353.png

 

 

0 件の賞賛
返信

2,159件の閲覧回数
CSBoy
Contributor II

hi,

I have compared your pictures, which are different from the installation package I downloaded. Mine is [S32r45_premium_Radar_SDk_evaluation_Package_0_8_0_220519.exe], and the size of the installation package is 74318KB.  So, where can I download the [S32R45_Preminum_Radar_SDK_080_220610] installation package.

thanks

タグ(1)
0 件の賞賛
返信

2,153件の閲覧回数
HaoRen
NXP Employee
NXP Employee

PRSDK is a paid software package.

The evaluation package is different from the complete package.

Could you tell me which customer you are?   This requires market support

0 件の賞賛
返信

2,131件の閲覧回数
CSBoy
Contributor II

Thank you.  if necessary, I'll contact nxp market.

0 件の賞賛
返信