S32R294_RSDK_1_3_0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R294_RSDK_1_3_0

2,243 Views
tyson1
Contributor I

Hi ,

    I installed the software for SWS32R294_Radar_SDK_1.3.0_D2105.exe in path C:\NXP

  But when I open the example in the S32 Design Studio for Power Architecture Version 2.1,create S32DS PROJECT FROM EXAMPLE ,import RSDK_Multi_RFE_example_S32R294,show File not found: /RSDK_Multi_RFE_example_S32R294/src/core0/main_c0.c.

The problem is that there are files in the RSDK path, but not in the workspace after import, so which step is wrong

Labels (1)
0 Kudos
Reply
4 Replies

2,062 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Latest info is that next release is in mid August and they will take care of the issue there.

Best regards,
Peter

0 Kudos
Reply

2,235 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

From your description it looks like all you need to do is to set correctly path to the source files in your project.

Could you post some screenshots of the errors?

Best regards,

Peter

0 Kudos
Reply

2,233 Views
tyson1
Contributor I

S32R294_RSDK__1_3_0   path in C:\NXP

 

0 Kudos
Reply

2,228 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I was talking with RSDK team, they will debug the issue in following days.

I will update you ASAP.

best regards,

Peter

0 Kudos
Reply