S32K312 Link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 Link

793件の閲覧回数
JCY1223
Contributor I

Hello:

I am now doing S32K312 software development, encountered the RAM is not enough to use, modify the configuration of the ld file, compile can pass, but the program can not run.

 

Configuration before modification:

int_sram : ORIGIN = 0x20400000, LENGTH = 0x0000E000 /* 56KB */
int_sram_fls_rsv : ORIGIN = 0x2040E000, LENGTH = 0x00000100
int_sram_stack_c0 : ORIGIN = 0x2040E100, LENGTH = 0x00001000 /* 4K */
int_sram_no_cacheable : ORIGIN = 0x2040F100, LENGTH = 0x00006E00 /* 24+3.5KB , needs to include int_results */
int_sram_results : ORIGIN = 0x20415F00, LENGTH = 0x00000100
int_sram_shareable : ORIGIN = 0x20416000, LENGTH = 0x00002000 /* 8KB */
ram_rsvd2 : ORIGIN = 0x20418000, LENGTH = 0 /* End of SRAM */

 

Modified configuration:

int_sram : ORIGIN = 0x20400000, LENGTH = 0x00013000 /* 76KB */
int_sram_fls_rsv : ORIGIN = 0x20413000, LENGTH = 0x00000100
int_sram_stack_c0 : ORIGIN = 0x20413100, LENGTH = 0x00001000 /* 4K */
int_sram_no_cacheable : ORIGIN = 0x20414100, LENGTH = 0x00002E00 /* 8+3.5KB , needs to include int_results */
int_sram_results : ORIGIN = 0x20416F00, LENGTH = 0x00000100
int_sram_shareable : ORIGIN = 0x20417000, LENGTH = 0x00001000 /* 4KB */
ram_rsvd2 : ORIGIN = 0x20418000, LENGTH = 0 /* End of SRAM */

 

How can I increase int_sram???

 

ラベル(1)
0 件の賞賛
返信
1 返信

773件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @JCY1223,

There can be problems with the MPU that is configured and enabled in system.c

Can you test it with the MPU disabled?

danielmartynek_0-1697185169071.png

 

Regards,

Daniel

 

 

0 件の賞賛
返信