S32K312 Autosar LCU example in EB Tresos and coding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 Autosar LCU example in EB Tresos and coding

2,070 Views
emerging
Contributor III

Hello Team,

Could someone please provide me an example for configuring LCU (Logic Control Unit) module in autosar s32k312 using EB Tresos

Thanks and regards

Labels (2)
Tags (2)
0 Kudos
Reply
3 Replies

2,051 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @emerging 

As you know, S32K3 has many derivatives, so to reduce effort, in the most recent RTD releases we only provide examples for K344, K358, K388, and K396. Examples of other derivatives can be created based on these existing examples.

With the RTDs comes an example code named Mcl_LcuControllMotor, which might be a good reference. Also, you can check the application note AN13884: 3-phase Sensorless PMSM Motor Control Kit with S32K344 using RTD Autosar API. 

Additionally, there is a thread that provides a training presentation related to the topic.

Complimentary PWM outputs - LCU configuration

 

B.R.

VaneB

0 Kudos
Reply

2,012 Views
emerging
Contributor III

Hello @VaneB ,

Could you please share me the download link of any RTDs comes with LCU module configuration and coding example.

Thanks and Regards

Tags (1)
0 Kudos
Reply

1,980 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @emerging 

The example Mcl_LcuControlMotor for EB Tresos is available for RTD version 3.0.0 P07 and 4.0.0. All the abailable RTD version can be download it from S32K3 Standard Software > Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M.

0 Kudos
Reply