S32K148EVB+ADTJA1101 use lwip sample code to collect data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K148EVB+ADTJA1101 use lwip sample code to collect data

1,298 次查看
gary_chiu
Contributor I

I use S32k148EVB+ADTJA1101-RMII module+lwip_s32k148 example to do ETHERNET function test, I use SocketTest v3.0.0 software to connect EVB and successfully send "11" data to EVB, the problem is that I have tried in ENET_DRV_ReadFrame(), enetif_input( ), there is no "11" when looking for buff data, what should I do to get the correct data?

标签 (1)
0 项奖励
回复
1 回复

1,234 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello,

By using ENET_DRV_ReadFrame() or enetif_input(), you will only be able to get the raw data of the buffer (i.e. encapsulated data, including upper layers e.g. data link, tcp, ip layer,...) To provide the fastest possible support, I'd like to you refer to the LwIP Application Developers Manual.

Best Regards,

Nam

0 项奖励
回复