[S32K148] how to receive multiple CAN ids from one MailBox.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[S32K148] how to receive multiple CAN ids from one MailBox.

跳至解决方案
3,809 次查看
HyungGyuKim76
Contributor I

Hi all,

As a test, Receiving two IDs(100, 101) normally with the code below.

#define RX_MAILBOX_0 0x0
#define RX_MAILBOX_1 0x1
#define RX_MSG_ID_0 (100UL)
#define RX_MSG_ID_1 (101UL)

int main(void)
{

................................................

/* Initialize Can0 */
CAN_Init(&can_pal1_instance, &can_pal1_Config0);

/* Configure RX buffer with index RX_MAILBOX */
CAN_ConfigRxBuff(&can_pal1_instance, RX_MAILBOX_0, &buffCfg, RX_MSG_ID_0);
CAN_ConfigRxBuff(&can_pal1_instance, RX_MAILBOX_1, &buffCfg, RX_MSG_ID_1); 
CAN_ConfigTxBuff(&can_pal1_instance, TX_MAILBOX_0, &buffCfg);
CAN_ConfigTxBuff(&can_pal1_instance, TX_MAILBOX_1, &buffCfg);

while(1)

{

memset(&recvMsg0, 0, sizeof(can_message_t));

CAN_Receive(&can_pal1_instance, RX_MAILBOX_0, &recvMsg0);
if(recvMsg0.data[0] != 0)
{uartPrintf(&uartStateTX, "CAN id : %x [0] : %d \r\n", recvMsg0.id, recvMsg0.data[0]);}

memset(&recvMsg1, 0, sizeof(can_message_t));
CAN_Receive(&can_pal1_instance, RX_MAILBOX_1, &recvMsg1);
if(recvMsg1.data[0] != 0)
{uartPrintf(&uartStateTX, "CAN id : %x [0] : %d [1] : %d \r\n", recvMsg1.id, recvMsg1.data[0]);}

}

}

But if I want to receive IDs from 100 to 200, do I have to receive 100 mailboxes?

Can you please tell me how to receive in one MailBox?

Please let me know if you have a simple example.

标签 (1)
0 项奖励
回复
1 解答
3,792 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi, 

you can config mask register and create some ID range to be received into given MB.
For example by clearing mask register (global or individual, depends what scheme you are using) you can receive all std. or ext. IDs into single MB.
Cleared bit in mask indicates corresponding received ID bit is don't care, otherwise it is compared with corresponding bit in ID in prepared MB.
For sure you cannot create any possible ID ranges, like your 100-200.

BR, Petr

在原帖中查看解决方案

标记 (1)
0 项奖励
回复
4 回复数
3,787 次查看
HyungGyuKim76
Contributor I

thank you.
I was able to get all the ids very simply by adding a single line as shown below.

FLEXCAN_DRV_SetRxMbGlobalMask(INST_CANCOM1, FLEXCAN_MSG_ID_STD, 0); // All id received masking

 

0 项奖励
回复
2,874 次查看
Dileep1441
Contributor I

Hi @HyungGyuKim76 

I'm facing the Same issue and trying to receive multiple CAN Messages, Can you please share your code.

and what are the settings need to change for this functionality.

 

Thanks in Advance.

0 项奖励
回复
3,059 次查看
akhilranga
Contributor IV

Hi there,

Can you please share the code with me. I just have the similar requirement. So, if you can share the code where you were able to get all the CAN ID's. 

标记 (1)
0 项奖励
回复
3,793 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi, 

you can config mask register and create some ID range to be received into given MB.
For example by clearing mask register (global or individual, depends what scheme you are using) you can receive all std. or ext. IDs into single MB.
Cleared bit in mask indicates corresponding received ID bit is don't care, otherwise it is compared with corresponding bit in ID in prepared MB.
For sure you cannot create any possible ID ranges, like your 100-200.

BR, Petr

标记 (1)
0 项奖励
回复