Hello All,
I'm working in S32K144 MCU for the FlexCAN Communication. I have used the Example Source NON-SDK for FlexCAN, EVB Board flashed the example and tap the CAN_TX Line(PTE5) to the scope and Running the programming can see the CAN Frame Data.
My problems are,
I'm using PTC3 -CAN_TX(ALT3) and PTC2-CAN_RX(ALT3) followed the same Example code only different is PORTC changed.
Please anyone faces the same problem with using PORT C for FlexCAN0
Port C Configuration,
Case 1:
PCC->PCCn[PCC_PORTC_INDEX ]|=PCC_PCCn_CGC_MASK; /* Enable clock for PORTC */
PORTC->PCR[3]|=PORT_PCR_MUX(3); /* Port C3: MUX = ALT3,(CAN0)C_CAN TX */
PORTC->PCR[2]|=PORT_PCR_MUX(3); /* Port C2: MUX = ALT3,(CAN0)C_CAN RX */
Case 2:
PCC->PCCn[PCC_PORTC_INDEX ]|=PCC_PCCn_CGC_MASK; /* Enable clock for PORTC */
PORTC->PCR[3] &= ~(PORT_PCR_MUX_MASK);
PORTC->PCR[3]|=PORT_PCR_MUX(3); /* Port C3: MUX = ALT3,(CAN0)C_CAN TX */
PORTC->PCR[2] &= ~(PORT_PCR_MUX_MASK);
PORTC->PCR[2]|=PORT_PCR_MUX(3); /* Port C2: MUX = ALT3,(CAN0)C_CAN RX */
Both Case 1 and Case2 i'm not see any Data signls with the scope.
Please let me know if any other configuration required.
Thanks,
Sakthivel K#
HI~
I have the same problem.
1. I made CAN0 OK on Demo board, and the CAN0 connects to PTE4 and PTE5
2. I moved codes to a new board,whose CAN0 connects to PTC2 and PTC3
3. I just changed CAN Interface SDK as follow:
After that, CAN0 can never work well, and PTC2 and PTC3 have no waves on scope
Is that anyone soveled this ?
Hi all,
I suppose that both of you are using S32K144 devkit.
On that board PTC3 is not connected to pin headers because it is by default connected to touch electrodes.
For more details about schematic please go to :S32K144 Evaluation Board|NXP and download S32K144 Quick Start Package.
Best regards,
Razvan
Hi Razvan,
I just ran the example projects "S32K144_Project_CanFd" and "S32K144_Project_FlexCan" on the evaluation board,
https://www.nxp.com/docs/en/quick-reference-guide/S32K144EVB-QSG.pdf
and found nothing from "PTE5" (CAN0_TX) mapped to header pin J6-18.
I am going to try these codes again.
Do you mind to help out please?
Thanks,
Kevin
Hi Kevin,
You don't find PTE5 pin on the pin header or you can't get CAN signal on that pin?
Also, from where did you get these examples? Did you tried CAN examples provided with SDK?
Best regards,
Razvan
Hi Razvan,
I found PTE5 pin on the pin header, and toggled this pin after I configured
it as a GPIO pin. Verified that is the right pin. I would like to find out
if there is a bit stream at this pin on the S32K144.
I can NOT find (see) CAN signal on this pin after I ran the example
programs.
Here are the schematic and layout for the board that I am using,
https://www.nxp.com/downloads/en/schematics/S32K144EVB-SCH-29248-RB1.pdf
https://www.nxp.com/docs/en/quick-reference-guide/S32K144EVB-QSG.pdf
I ran the examples from S32K1xx_cookbook, these are attached.
Also I imported examples from S32 Design Studio, and found no bit stream on
CAN0_Tx ( PTE5).
Please help,
Thanks,
Kevin
On Wed, Mar 20, 2019 at 2:58 AM razva_tilimpea <admin@community.nxp.com>