S32K144 CSEc Engine usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 CSEc Engine usage

2,250 Views
harish_g2
Contributor II

Hi All,

We are trying to use CSEc engine for AES 128 encoding. In the example code, board is resetting after calling this function. 

/* Initialize Flash for CSEc operation */
initFlashForCsecOperation();

We just wanted to do AES 128 bit encoding.

Please let us know how it can be done.

Regards,

Harish G

0 Kudos
Reply
2 Replies

2,018 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Harish G

Please remember that Flash partitioning for CSEc operation must only be run with RAM configuration. The first time when running the example on the board (or after a key erases) should be run from RAM, in order to enable CSEc operation.

I recommend you check the application note AN5401:

https://www.nxp.com/webapp/Download?colCode=AN5401 

Hope this helps
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply

1,654 Views
luyu
Contributor I

Hello 

        I met  the same issue as the customer did. And of course we know it should run in RAM.

        But when using IAR for the example, and if using the Ram icf ,it could be ok

        And when using the flash icf for download, actually it will happen same issue as the customer did.

        I tried set __ramfunc for the initFlashForCsecOperation, but it doesn't work. 

        Did you try using the flash icf file for the example?

0 Kudos
Reply