S32K142_64PIN ADC0 Processer Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K142_64PIN ADC0 Processer Expert

8,120 次查看
314404229
Contributor I

I use S32K142_64pin, ADC0 channel15.

Processer Expert Problem: ADC1 of S32K142_64 has only 11 external input channels.

But ADC0 has 15 external input channels.

I's it a BUG?

How to solve it.

标记 (3)
0 项奖励
回复
2 回复数

1,877 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I am able to select ADC0_CH15 of S32K142_64pin.

You may need to change package, please refer: How to change package on S32DS Processor Expert

S32K142_64 ADC0_CH15.png

ADC0_SE15.png

 

The adc_hwtrigger_s32k142 example is from RTM3.0.0

adc_hwtrigger_s32k142.png

For S32K1xx, the recommended SDK version to use is S32K1xx SDK RTM3.0.0 with UP10(SR3.0.1) and 11(SR3.0.2) installed;

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,877 次查看
314404229
Contributor I

Thank U. It need to update the SDK.

0 项奖励
回复