S32K118FTM组件输出PWM问题

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K118FTM组件输出PWM问题

1,086 次查看
GAC-Lamp-Knight
Contributor II

如果要使用S32K118的一个模组,例如FTM0,使用它的不同通道,如CH0和CH5输出不同频率输出PWM,应该如何实现。

标签 (1)
标记 (4)
0 项奖励
回复
1 回复

1,071 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Regarding your question…

[Google translation]
"S32K118FTM component output PWM problem

If you want to use a module of S32K118, such as FTM0, use its different channels, such as CH0 and CH5 to output PWM at different frequencies, how should it be implemented."

The FlexTimer Module (FTM) does not allow using different frequencies between channels of the same instance. If you need different PWM frequencies you will have to use different instances of FTM.

Hope it helps you.

Have a nice day!

0 项奖励
回复
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----