S32K118 recovery on debug connection failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K118 recovery on debug connection failure

跳至解决方案
1,845 次查看
wei_w_he
Contributor IV

Dear Officer,

We had a SK32K118 EVB board working fine previous, then after playing around with the "CAN bootloader" project then suddenly we are not able to connect with the board via "OpenSDA Embedded -USB Port". (We will always jump to P&E assistant popup then failed on connection.)

After searching around, it seems some memory has been corrupted? And how can we recover from this case? Any method to performa a entire re-falsh the chip?

Tks and best regards

He Wei

 

标签 (1)
0 项奖励
1 解答
1,785 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Dear He Wei,

 

Thank you for the information.

Unfortunately, there can be many causes. It is hard to say if just an SBC chip or the whole board is damaged.

 

Best regards,

Diana

在原帖中查看解决方案

6 回复数
1,836 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello He Wei,

 

Can you share the PrintScreen of the failure?

Can you tell me the state of LED D1 located on the board?

Please, restart S32DS/PC and try to create a new empty project and select the option below in the debug configuration.

dianabatrlova_0-1607349710291.png

 

Best regards,

Diana

0 项奖励
1,825 次查看
wei_w_he
Contributor IV

Dear Diana,

1). The error print is:

wei_w_he_0-1607390759053.png

2) LED D1 is always off. (Further, D2 and D3 will be On if selecting 3.3V but D3 will be off if selecting 5V)

3) I create a empty S32K118 project and select the option as you recommend, the same error appear.

4) Further, also we connected with a multilink device and try the "USB Multilink-USB port" option but got same error too.

Please advise.

Tks and best regards

He Wei

 

 
 

 

 

 

 

 

 

0 项奖励
1,814 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

When powered through USB, LEDs D2 and D3 should light green, also, in the case of selecting 5V.

Can you, please, measure VDD_MCU whether the MCU is powered (in both cases)?

 

Can you share the last project which you loaded into MCU and S32DS version? (I can try to reproduce your issue)

 

Thank you.

Best regards,

Diana

0 项奖励
1,792 次查看
wei_w_he
Contributor IV

Dear Diana,

We measured VDD_MCU and it always LOW (0 Vol) no matter powered from USB (5V or 3V) or external 12V, it shows the MCU itself could be permanently damaged.

BR

He Wei

 

0 项奖励
1,786 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Dear He Wei,

 

Thank you for the information.

Unfortunately, there can be many causes. It is hard to say if just an SBC chip or the whole board is damaged.

 

Best regards,

Diana

1,807 次查看
wei_w_he
Contributor IV

Dear Diana,

I will ask my colleague to do the measurement as you mentioned. and I just quickly share what we did to "spoil" this board:

1. We build the " S32K118_CAN_bootloader" from NXP.

2. We go to "Run-> Flash from file.." option to load the ELF file.

Is the issue caused by "Flash from file.."?

Tks nad best regards

He Wei

 

0 项奖励