S32K SDK can_pal lack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K SDK can_pal lack

ソリューションへジャンプ
2,377件の閲覧回数
adria
Contributor I

Hi,

I am usign processor expert and have added can_pal component to my project. I see there are some features from FlexCAN which can_pal doesn't cover. If I want to use them, what do you recommend me to do:

1. Keep using can_pal and, in case I want to use some of the FlexCAN functions which are not covered by can_pal, directly call those FlexCAN function.

2. Remove can_pal component from my project and start using only FlexCAN.

Best regards,

Adria

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,160件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Adria,

If your application allows you to use FlexCAN instead of can_pal, my recommendation would be to stick to your second option, remove can_pal component from your project and start using only FlexCAN.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,161件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Adria,

If your application allows you to use FlexCAN instead of can_pal, my recommendation would be to stick to your second option, remove can_pal component from your project and start using only FlexCAN.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信