Hi all,
there is an issue with the pin muxing configuration tool in S32DS3.2 when selecting S32K314 and with MAXQFp100 package. Using RTD 0.8.1
If you chose MAXQFP100 then still the MAXQFP172 is displayed and the pinmuxing settings do not reflect the 100pin version. Also the picture of MAXQFP172 is not shown correctly.
Thanks for checking and correction.
MAXQFP172:
MAXQFP100:
br
Guenter