S32DS with MPC5744P SDK, linker error and which version.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS with MPC5744P SDK, linker error and which version.

1,208 次查看
eddyderick
Contributor I

Hello,

I am currently developing for the MPC5744P platform using S32DS and the latest upgrade.

When I generate my project including the  "MPC5744P_SDK_Z4_GCC" version 0.8.2, the generated linker file is wrong.

It is using a m_text of length 2560K while it should be 2048K.

I have checked all the files I have and found two wrong linker files in the following directories:

- C:\NXP\S32DS_Power_v2017.R1\S32DS\S32_SDK_MPC574xx_EAR_0.8.2\platform\devices\MPC5744P\linker\ghs

- C:\NXP\S32DS_Power_v2017.R1\S32DS\S32_SDK_MPC574xx_EAR_0.8.2\platform\devices\MPC5744P\linker\gcc

Another question is, which SDK should I include for the MPC5744P to release a production ready software?

I am using GCC as compiler.

Regards,

Eddy DERICK

标签 (1)
0 项奖励
回复
1 回复

1,060 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

on my S32DS installation is the m_text section length 2048K

pastedImage_1.png

This file is linked by default and if you did some changes in other project - the change affects all existing and newly created projects. 

For release purpose you can use RTM SDK version - latest one is S32PA RTM SDK v2.0.0

Jiri 

0 项奖励
回复