Hello.
To create IAR SDK project, do I need to install IAR 7.x?
I just installed IAR 8.x at my laptop.
but, if I create S32DS project based on 'IAR 8.x toolchain' there is no selectable SDK list.
if I create 'IAR 7.x- SDK' project, S32DS shows error finding IAR 7.x toolchain. (But, I didn't installed it.)
So, I wonder I must install IAR 7.x to create SDK project at S32DS.
Added with it, is there approximate schedule to support IAR 8.x SDK?
Best Regards,
Mac.
 
					
				
		
 raresvasile
		
			raresvasile
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Mac,
What version of S32 SDK you have installed in S32 DS? S32 SDK supports IAR 8.11.2 starting from BETA 1.9.0.
Best regards,
Rares
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello. Mike.
I am using S32K144
Best Regards,
Mac.
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello jongcheonkim,
When you used the New Project Wizard, did you select the correct Toolchain option as below?
After selecting the correct toolchain, then click next and you should be able to select the SDK.
Please let me know if this does not resolve your issue.
Best Regards,
Mike
Hello. Mike.
Sorry, I missed my 'S32DS for ARM installation details related IAR' for your reference.
Best Regards,
Mac.
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Mac,
Unfortunately, if this is an issue related to the IAR plugin, then I cannot provide much help. You will need to contact IAR for support with that. It is a good idea to have all of the updates installed.
You must have IAR EW installed with a valid license.
Hope it helps,
Mike
Hello. Mike.
Thank you so much for your help.
After I select IAR 8.x Toolchain, there is no SDK list.
I think that it may comes from during install S32DS update related IAR, I have some errors.
Do you have any idea how can I avoid it?
This is about my S32DS for ARM information
Best Regards,
Mac.