S32DS and IAR toolchain support SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS and IAR toolchain support SDK

3,483 次查看
jongcheonkim
Contributor II

Hello.

To create IAR SDK project, do I need to install IAR 7.x?

I just installed IAR 8.x at my laptop.

but, if I create S32DS project based on 'IAR 8.x toolchain' there is no selectable SDK list.

if I create 'IAR 7.x- SDK' project, S32DS shows error finding IAR 7.x toolchain. (But, I didn't installed it.)

So, I wonder I must install IAR 7.x to create SDK project at S32DS.

Added with it, is there approximate schedule to support IAR 8.x SDK?

Best Regards,

Mac.

标记 (4)
0 项奖励
回复
7 回复数

2,955 次查看
raresvasile
NXP Employee
NXP Employee

Hi Mac,

What version of S32 SDK you have installed in S32 DS? S32 SDK supports IAR 8.11.2 starting from BETA 1.9.0.

Best regards,

Rares

0 项奖励
回复

2,956 次查看
mikedoidge
NXP Employee
NXP Employee

Hello jongcheonkim‌,

Which MCU are you using?

Mike

0 项奖励
回复

2,956 次查看
jongcheonkim
Contributor II

Hello. Mike.

I am using S32K144

Best Regards,

Mac.

0 项奖励
回复

2,956 次查看
mikedoidge
NXP Employee
NXP Employee

Hello jongcheonkim‌,

When you used the New Project Wizard, did you select the correct Toolchain option as below?

pastedImage_2.pngpastedImage_1.png

After selecting the correct toolchain, then click next and you should be able to select the SDK.

pastedImage_3.png

Please let me know if this does not resolve your issue.

Best Regards,

Mike

2,956 次查看
jongcheonkim
Contributor II

Hello. Mike.

Sorry, I missed my 'S32DS for ARM installation details related IAR' for your reference.

pastedImage_1.png

Best Regards,

Mac.

0 项奖励
回复

2,956 次查看
mikedoidge
NXP Employee
NXP Employee

Hi Mac,

Unfortunately, if this is an issue related to the IAR plugin, then I cannot provide much help. You will need to contact IAR for support with that. It is a good idea to have all of the updates installed.

You must have IAR EW installed with a valid license.

Hope it helps,

Mike

0 项奖励
回复

2,956 次查看
jongcheonkim
Contributor II

Hello. Mike.

Thank you so much for your help.

After I select IAR 8.x Toolchain, there is no SDK list. 

S32DS_S32K144_IAR8x_ToolChain.PNG

S32DS_S32K144_IAR8x_SDKList.PNG

I think that it may comes from during install S32DS update related IAR, I have some errors.

Do you have any idea how can I avoid it?

pastedImage_6.png

pastedImage_8.png

pastedImage_9.png

This is about my S32DS for ARM information

pastedImage_10.png

Best Regards,

Mac.

0 项奖励
回复