S32DS SDK S32K1xx RTM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS SDK S32K1xx RTM

Jump to solution
10,819 Views
koehlerl
Contributor IV

I can't install the SDK S32K1xx RTM. I get an error message.

Br lutz

0 Kudos
Reply
1 Solution
10,131 Views
koehlerl
Contributor IV

The online update from SDK S32K1xx 3.0 RTM works now.

BR Lutz

Von: stanish

Gesendet: Montag, 4. März 2019 16:18

An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>

Betreff: Re: - Re: S32DS SDK S32K1xx RTM

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: S32DS SDK S32K1xx RTM

reply from Stanislav Sliva<https://community.nxp.com/people/stanish?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1120147?commentID=1120147&et=watches.email.thread#comment-1120147>

View solution in original post

0 Kudos
Reply
4 Replies
10,130 Views
stanish
NXP Employee
NXP Employee

Hi Lutz,

Could you possibly attach screenshot with an error you get?

Which version of S32DS are you using?

Which RTM version are you trying to install?

Currently the latest RTM version for S32K1xx is S3214x SDK RTM 2.0.0.

https://community.nxp.com/docs/DOC-340989 

You can install it by online/offline method. Could you possibly try the other method?

Stan

0 Kudos
Reply
10,130 Views
koehlerl
Contributor IV

Hi,

check for updates says, there is a newer version SDK S32K1xx 3.0 RTM

The Error:

BR Lutz

Von: stanish

Gesendet: Montag, 4. März 2019 14:00

An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>

Betreff: Re: - Re: S32DS SDK S32K1xx RTM

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: S32DS SDK S32K1xx RTM

reply from Stanislav Sliva<https://community.nxp.com/people/stanish?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1119965?commentID=1119965&et=watches.email.thread#comment-1119965>

0 Kudos
Reply
10,130 Views
stanish
NXP Employee
NXP Employee

Thank you for the report.

We are now investigating this issue.

Could you possibly download the offline update archive and install it using offline method?

Please let me know if the workaround works for you.

BR,

Stan

0 Kudos
Reply
10,132 Views
koehlerl
Contributor IV

The online update from SDK S32K1xx 3.0 RTM works now.

BR Lutz

Von: stanish

Gesendet: Montag, 4. März 2019 16:18

An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>

Betreff: Re: - Re: S32DS SDK S32K1xx RTM

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: S32DS SDK S32K1xx RTM

reply from Stanislav Sliva<https://community.nxp.com/people/stanish?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1120147?commentID=1120147&et=watches.email.thread#comment-1120147>

0 Kudos
Reply