The online update from SDK S32K1xx 3.0 RTM works now.
BR Lutz
Von: stanish
Gesendet: Montag, 4. März 2019 16:18
An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>
Betreff: Re: - Re: S32DS SDK S32K1xx RTM
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: S32DS SDK S32K1xx RTM
reply from Stanislav Sliva<https://community.nxp.com/people/stanish?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1120147?commentID=1120147&et=watches.email.thread#comment-1120147>
Hi Lutz,
Could you possibly attach screenshot with an error you get?
Which version of S32DS are you using?
Which RTM version are you trying to install?
Currently the latest RTM version for S32K1xx is S3214x SDK RTM 2.0.0.
https://community.nxp.com/docs/DOC-340989
You can install it by online/offline method. Could you possibly try the other method?
Stan
Hi,
check for updates says, there is a newer version SDK S32K1xx 3.0 RTM
The Error:
BR Lutz
Von: stanish
Gesendet: Montag, 4. März 2019 14:00
An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>
Betreff: Re: - Re: S32DS SDK S32K1xx RTM
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: S32DS SDK S32K1xx RTM
reply from Stanislav Sliva<https://community.nxp.com/people/stanish?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1119965?commentID=1119965&et=watches.email.thread#comment-1119965>
Thank you for the report.
We are now investigating this issue.
Could you possibly download the offline update archive and install it using offline method?
Please let me know if the workaround works for you.
BR,
Stan
The online update from SDK S32K1xx 3.0 RTM works now.
BR Lutz
Von: stanish
Gesendet: Montag, 4. März 2019 16:18
An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>
Betreff: Re: - Re: S32DS SDK S32K1xx RTM
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: S32DS SDK S32K1xx RTM
reply from Stanislav Sliva<https://community.nxp.com/people/stanish?et=watches.email.thread> in S32 Design Studio - View the full discussion<https://community.nxp.com/message/1120147?commentID=1120147&et=watches.email.thread#comment-1120147>