S32DS 3.5 building issue with s32k116 Hello World example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS 3.5 building issue with s32k116 Hello World example

跳至解决方案
1,761 次查看
NicoloStrozzi
Contributor III

Hello all,

I've moved to the S32DS 3.5 after few years using S32DS 2.2 IDE. After installing all SDK and all Update package, I'm trying to build the examples and flash them on a s32k116 EVB.

Unfortunately the building shows error an is not completed. In the following I add the details:

EXAMPLE NAME: hello_world_s32k116

TOOLCHAIN: NXP GCC 6.3 for Arm 32-bit Bare-Metal

ERRORS:

NicoloStrozzi_0-1705482841544.png

CONSOLE:

10:01:35 **** Incremental Build of configuration Debug_FLASH for project hello_world_s32k116 ****
make -j16 all
Building file: ../src/main.c
Building file: ../board/clock_config.c
Building file: ../board/pin_mux.c
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@board/clock_config.args" -MMD -MP -MF"board/clock_config.d" -MT"board/clock_config.o" -o "board/clock_config.o" "../board/clock_config.c"
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@board/clock_config.args" -MMD -MP -MF"board/pin_mux.d" -MT"board/pin_mux.o" -o "board/pin_mux.o" "../board/pin_mux.c"
arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"
arm-none-eabi-gcc.exe: error: nano.specs: No such file or directory
make: *** [board/subdir.mk:23: board/clock_config.o] Error 1
make: *** Waiting for unfinished jobs....
arm-none-eabi-gcc.exe: error: nano.specs: No such file or directory
make: *** [board/subdir.mk:23: board/pin_mux.o] Error 1
Building file: C:/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/platform/drivers/src/pins/pins_driver.c
arm-none-eabi-gcc.exe: error: nano.specs: No such file or directory
make: *** [src/subdir.mk:20: src/main.o] Error 1
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/drivers/src/pins/pins_driver.args" -MMD -MP -MF"SDK/platform/drivers/src/pins/pins_driver.d" -MT"SDK/platform/drivers/src/pins/pins_driver.o" -o "SDK/platform/drivers/src/pins/pins_driver.o" "C:/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/platform/drivers/src/pins/pins_driver.c"
arm-none-eabi-gcc.exe: error: nano.specs: No such file or directory
make: *** [SDK/platform/drivers/src/pins/subdir.mk:23: SDK/platform/drivers/src/pins/pins_driver.o] Error 1
"make -j16 all" terminated with exit code 2. Build might be incomplete.

10:01:36 Build Failed. 5 errors, 0 warnings. (took 584ms)

 

 

标签 (1)
0 项奖励
回复
1 解答
1,750 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version. Do not use S32K1 SDK 4.0.1 with S32DS v3.5.
It is recommended to install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4.
Or install S32K1 RTD 2.0.x with S32DS Extensions and Updates in S32DS v3.5.
 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,751 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version. Do not use S32K1 SDK 4.0.1 with S32DS v3.5.
It is recommended to install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4.
Or install S32K1 RTD 2.0.x with S32DS Extensions and Updates in S32DS v3.5.
 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,693 次查看
NicoloStrozzi
Contributor III

Thank you Robin, 

this was exactly the issue. My mistake rises because while installing S32DS v3.5 the proposed SDK version is RTM 4.0.1 which is not working. 

0 项奖励
回复