S32 SDK for S32R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 SDK for S32R

3,844 Views
huangwilliam
Contributor I

Dear Sir,

             May I know the available schedule for S32 SDK for S32R?

Many thanks for your helps.

BR

William Huang

Labels (1)
5 Replies

3,149 Views
allenyu
Contributor II

Hi,

The SDK support Ethernet? What is the corresponding ENET PHY? TJA1102?

0 Kudos
Reply

3,149 Views
stanish
NXP Employee
NXP Employee

Hi William,

the internal teams are currently working to finalize the roadmap for this part (I assume you mean S32R274).

But the release of EAR (Early Access Release) it is currently anticipated at the end of 2017 or 1Q2018

regards,

Stan

3,149 Views
ruifengdu
Contributor I

Hi Stan,

     May I know the SDK for S32R274 is available now? if is available, where can I download it, thank u & best wishes.

0 Kudos
Reply

3,149 Views
stanish
NXP Employee
NXP Employee

Hi,

According to the latest information I have the S32R274 SDK should be released  in Jun-2018 time frame.

S.

0 Kudos
Reply

3,149 Views
huangwilliam
Contributor I

Hi Stan,

             Understood and thanks for your information. 

BR

William Huang

0 Kudos
Reply