S32 SDK 0.8.4 in S32 Design Studio for ARM v2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 SDK 0.8.4 in S32 Design Studio for ARM v2.0

1,707件の閲覧回数
mauromarinoni
Contributor I

I've tried to install the different versions of S32 for Linux (i.e., 2018R1, v2.0, v1.3) but I was not able to install the SDK (in particular version 0.8.4 from v2.0). In the end, I was forced to grab it from a Windows installation where the folder is present.

I've missed some options to flag during the installation procedure? Or it's the desired result to avoid the SDK installation in Linux? 

タグ(3)
0 件の賞賛
返信
1 返信

1,577件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately SDK is not supported on Linux host. 

Jiri

0 件の賞賛
返信