Re: Require procedure for using the SDK RTM V3.0.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: Require procedure for using the SDK RTM V3.0.3

1,461 Views
vijaysubramanian
Contributor I

Hi,

I am getting the below error, while Installing the software KSDK 1.1.0

 

An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=null --> [R]com.freescale.processorexpert.ksdk-1.1.0.sp_root 1.0.0.b141204, action=).
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.

Could you pls provide the solution.

 

0 Kudos
Reply
1 Reply

1,026 Views
mohammad_saad
Contributor I

@addiyi 
I'm facing the same problem as well.
Can you please help resolve this issue?

0 Kudos
Reply