PlatformSDK_S32XX_4_0_0_S32G274A_Rev2_M7_0_4.0.0_PATH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PlatformSDK_S32XX_4_0_0_S32G274A_Rev2_M7_0_4.0.0_PATH

551 Views
mmoi
Contributor II

I installed the LLCE software as per the manual, and the can2can routine that opened llce's S32G2 after my installation was done said there was an error “ Description Resource Path Location Type
SDK PlatformSDK_S32XX_4_0_0_S32G274A_Rev2_M7_0_4.0.0_PATH is not found in workspace Can_Llce_DS_Can2Can_S32G274A_M7 P/Can_Llce_DS_Can2Can_S32G274A_M7 Missed SDK Marker

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

282 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your S32DS version? Do you have installed S32G2 RTD v4.0.0?

0 Kudos
Reply