Missing file in RTM 3.0.0 EEPROM Emulation driver demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing file in RTM 3.0.0 EEPROM Emulation driver demo

Jump to solution
2,659 Views
morrisli
Contributor I

Hi all,

    I am studying the EEPROM emulation middleware. It was found a demo project in S32_SDK_RTM 3.0.0. The project defined configurations in the file "eee1.h"  However, the file could not be found the SDK folder. Could anybody provide this file?

Regards,

Morris 

Labels (1)
0 Kudos
Reply
1 Solution
2,637 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

"eee1.h" and "eee1.c" are generated files and appears in project's "Generated_Code" folder upon Procesor Expert generates a code.

 

BR, Petr

 

View solution in original post

0 Kudos
Reply
4 Replies
2,638 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

"eee1.h" and "eee1.c" are generated files and appears in project's "Generated_Code" folder upon Procesor Expert generates a code.

 

BR, Petr

 

0 Kudos
Reply
2,630 Views
morrisli
Contributor I

Hi Petr,

    It seems S32DS V1.2 could not generate these files for the MCU S32R372. I modified the file from generated code for MPC574x and it was worked. Thanks for your help. 

BR,

Morris

0 Kudos
Reply
2,646 Views
morrisli
Contributor I

Hi Daniel,

The MCU is S32R372. The IDE is S32DS v1.2.

Regards,

Morris

0 Kudos
Reply
2,654 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Morris,

Please specify the MCU and the S32 Desing Studio version,

Thank you,

BR, Daniel

 

0 Kudos
Reply