LPSPI after Lpspi_Ip_AsyncTransmit stays in BUSY state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI after Lpspi_Ip_AsyncTransmit stays in BUSY state

Jump to solution
3,266 Views
sstelmak
Contributor III

Lpspi_Ip_AsyncTransmit() call gets executed once with expected  SPI waveforms.

Other calls are rejected because drives stays in LPSPI_IP_BUSY state.

I have a workaround to call Lpspi_Ip_Cancel() when BUSY state is reported:

if (Lpspi_Ip_GetStatus() == LPSPI_IP_BUSY) Lpspi_Ip_Cancel();

Lpspi_Ip_AsyncTransmit();

This works but I won't want to keep using that cancel call.

What can keep driver in BUSY state even after all needed data are properly Tx/Rx by SPI?

I use RTD 4.0.0, SPI with Tx/Rx DMA channels. DMA does not have global/transfer/scatter configs, also no interrupt callback.

 

 

Labels (1)
0 Kudos
Reply
1 Solution
2,225 Views
sstelmak
Contributor III

I ended up with writing my own function using synchronous transmit as example. It was possible to use fifo and have function that does not use interrupts(well, almost) and dma and returns immediately. That works similar to Lpspi_Ip_AsyncTransmit for my project.

View solution in original post

8 Replies
2,226 Views
sstelmak
Contributor III

I ended up with writing my own function using synchronous transmit as example. It was possible to use fifo and have function that does not use interrupts(well, almost) and dma and returns immediately. That works similar to Lpspi_Ip_AsyncTransmit for my project.

2,238 Views
prasadrashinkar
Contributor II

Hello Daniel,

We have the same issue For S32k44, configured LPSPI using EB tresos and tried to transmit data using Lpspi_Ip_AsyncTransmit()

call gets executed once Other calls are rejected because the drives stays in LPSPI_IP_BUSY state .

Can please share Example project of S32K344(with EB tresos configuration) for Lpspi_Ip_AsyncTransmit(); using Dma ?

 

0 Kudos
Reply
2,231 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Please create a new thread,

 

Thank you,

Daniel

0 Kudos
Reply
3,246 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @sstelmak,

I understand the driver never becomes IDLE after the transfer.

It would help if you could share the project so that I can test it.

Did you enable DMA interrups in the IntCtrl_Ip driver?

 

Regards,

Daniel

0 Kudos
Reply
3,235 Views
sstelmak
Contributor III

Hello,

I can't post entire project per company policies, it would be ok to email it directly.

Attached is the mex and few relevant c files. 

DMA or SPI interrupts are not configured. This is because I have restriction for micro throughput and looking for possibility to skip unnecessary calls.

 

0 Kudos
Reply
3,224 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @sstelmak,

The driver requires the DMA interrupts.

Have a look at the Lpspi_Flexio_Ip_Transfer_S32K344 example, where the FlexIO_SPI driver uses DMA.

 

BR, Daniel

0 Kudos
Reply
3,202 Views
sstelmak
Contributor III

Hello,

I added DMA ISRs (I use same DMA channels as the example) to IntCtrl_Ip

sstelmak_1-1721932993339.png

Nothing changed after that, and I didn't see that any of those interrupts were called.

 

 

 

 

0 Kudos
Reply
3,185 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Try enabling Global config in the in the DMA driver.

Please share the whole project (or a test project that can demonstrate the issue,) so that I can test it.

 

 

Thank you,

BR, Daniel

0 Kudos
Reply