Issue of creating S32V234 APEX_graph

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue of creating S32V234 APEX_graph

493件の閲覧回数
751301185
Contributor II

微信图片_20200624151648.png

After I connected the kernel in Vision Graph and selected Processes in APEX2 Program Diagram, how should I choose Inlets (Image Inlet? or Number Inlet? or Pointer Inlet?), Outlets (Image Outlet? or Number Outlet ? or Pointer Outlet?)?

Can anyone help me analyze?

0 件の賞賛
1 返信

435件の閲覧回数
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem modules is done only
via tickets. This Community is not appropriate for questions of this kind.  If you wish NXP

Technical Support to help you with this issue, please open a Support Case


Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛