Hi
Example S32K144 FlexCAN Pretended Networking STOP mode test S32DS.ARM.2.2
Please check "55.5.5 Receive process under Pretended Networking mode" of S32K1xx MCU Family - Reference Manual:
Pretended Networking mode adds specific wakeup functionality in low power mode (Stop mode). When Pretended Networking mode (PN) is enabled by asserting MCR[PNET_EN], FlexCAN continues processing Rx CAN messages under low power mode, and is able to detect specific wakeup messages by filtering them against ID and payload target values using preselected matching criteria. Wakeup functionality is not available for messages in CAN FD format. When in Pretended Networking mode, CAN FD format messages are ignored.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------