Is it possible to generate different frequency on each channel on same Eioms instance?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to generate different frequency on each channel on same Eioms instance?

2,329件の閲覧回数
PratikY
Contributor II

Hello @PetrS ,

I am using the S32K344EVB-Q257 board. Can I generate different frequencies on each channel of the same EMios instant?

Ex : On Emios Instance 1 channel 22 should generate 1000Hz and channel 23 should generate 2000Hz,is it possible?

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,316件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, it is possible for mentioned channels.
eMIOS ch22 and ch23 are Type X channels, so having its internal counter. Can be configured for OPWFMB mode, thus can have its own generated PWM freq.

BR, Petr

0 件の賞賛
返信

2,309件の閲覧回数
PratikY
Contributor II

Hi, @PetrS Thanks for the quick response.

I am able to generate different frequency signals at 22 and 23 channels, but I am asking in general, Is it possible to configure different frequencies from any channel from 0 to 23?

 

0 件の賞賛
返信

2,305件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no, it is not.
See my reply for similar question on https://community.nxp.com/t5/S32K/S32K344-hardware-PWM-frequency/m-p/1401775

BR, Petr

 

0 件の賞賛
返信

2,288件の閲覧回数
PratikY
Contributor II

Hi @PetrS , Thanks for the reply.

So as per my understanding, I should be able to generate unique frequency on each channel which OPWFMB Mode, which includes following chanells 

Emios 0
CH0,Ch8,Ch16,CH22,CH23, CH1-CH7

Emios 1 and Emios 2
CH0,Ch8,Ch16,CH22,CH23

Is it correct?

0 件の賞賛
返信

2,281件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

yes, correct,

BR, Petr

0 件の賞賛
返信