Incorrect port definitions in SDK for (at least) MPC5745R

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Incorrect port definitions in SDK for (at least) MPC5745R

1,326 次查看
joost_sannen
Contributor I

I believe I have found a problem with the port definitions in the SDK for the MPC5745R.
From port PTK all pointers actually reference PTJ...

After applying the patch below things seem better. Could someone please confirm this is a bug and that my fix is correct and complete?

Patch:

Index: MPC5745R_features.h
===================================================================
--- MPC5745R_features.h (revision 1053)
+++ MPC5745R_features.h (revision 1082)
@@ -1752,27 +1752,27 @@
/** Peripheral PTK base address */
#define PTK_BASE (0xFFFC1714u)
/** Peripheral PTK base pointer */
-#define PTK ((GPIO_Type *)PTJ_BASE)
+#define PTK ((GPIO_Type *)PTK_BASE)
/** Peripheral PTL base address */
#define PTL_BASE (0xFFFC1716u)
/** Peripheral PTL base pointer */
-#define PTL ((GPIO_Type *)PTJ_BASE)
+#define PTL ((GPIO_Type *)PTL_BASE)
/** Peripheral PTW base address */
#define PTW_BASE (0xFFFC1718u)
/** Peripheral PTW base pointer */
-#define PTW ((GPIO_Type *)PTJ_BASE)
+#define PTW ((GPIO_Type *)PTW_BASE)
/** Peripheral PTX base address */
#define PTX_BASE (0xFFFC171Au)
/** Peripheral PTX base pointer */
-#define PTX ((GPIO_Type *)PTJ_BASE)
+#define PTX ((GPIO_Type *)PTX_BASE)
/** Peripheral PTY base address */
#define PTY_BASE (0xFFFC171Cu)
/** Peripheral PTY base pointer */
-#define PTY ((GPIO_Type *)PTJ_BASE)
+#define PTY ((GPIO_Type *)PTY_BASE)
/** Peripheral PTZ base address */
#define PTZ_BASE (0xFFFC171Eu)
/** Peripheral PTZ base pointer */
-#define PTZ ((GPIO_Type *)PTJ_BASE)
+#define PTZ ((GPIO_Type *)PTZ_BASE)

/** Array initializer of GPIO peripheral base addresses */
#define GPIO_BASE_ADDRS { PTA_BASE, PTB_BASE, PTC_BASE, PTD_BASE, \

标签 (1)
0 项奖励
回复
1 回复

1,140 次查看
cezardobromir
NXP Employee
NXP Employee

Hello Joost,

Indeed, it seems to be an issue in the SDK pointers definitions.

Thank you for reporting the issue. We will have it fixed for the next release.

Until then please use the fixed patch that you mentioned.

Best regards,

Cezar

0 项奖励
回复