ISELED SDK 4.0.1 example show SDK S32K144_SDK_4.0.0_PATH is not found in workspace

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISELED SDK 4.0.1 example show SDK S32K144_SDK_4.0.0_PATH is not found in workspace

5,447 Views
Kris_Ke
Contributor III

Dear 

I use S32K144 ULVLL and S32 Platform v3.4 for ISELED Development, but it can't burn and execute normally, stuck in reset all the time.

01.png

 

I have updated to the latest and still have problems.

I tried to check the Linked resources and found that the SDK library "libiseled_S32K144.a" is incorrectly configured.

 

02.png

 

But the actual installation directory is C:\nxp\S32DS.3.4\S32DS\software\S32SDK_S32K1XX_RTM_4.0.1\platform\drivers\src\iseled\gcc

03.png

 

 

When the SDK example is loaded for the first time and Build it, there will be no problems.

04.png

 

And there is no problem with the SDK configuration in Properties.

05.png

 

But when I close S32 Platform v3.4 and reopen it, there will be SDK S32K144_SDK_4.0.0_PATH is not found in workspace error

06.png

 

When opening Properties, SDK 4.0.0 error will always appear, but there is no SDK 4.0.0 configuration at all.

07.png

 

After pressing Yes, the error still exists and the program cannot be executed normally.

 

 

There is another problem. I use ftm_period_interrupt_s32K144 cannot be executed normally, but ftm_period_interrupt_s32K144W can be executed normally.

 

Please help confirm the above two questions

 

 

Thanks,

Kris

 

 

 

 

0 Kudos
Reply
4 Replies

5,267 Views
Guille1
Contributor I

Hi kresse,

Thank you very much for your answer, she has been very helpful

Guille.

 

0 Kudos
Reply

5,303 Views
Guille1
Contributor I

Hi Kris,
I have the same problem "SDK S32K116_SDK_4.0.0_PATH" not found in workspace. Could you finally figure it out?

Thanks,

 Guille.

0 Kudos
Reply

5,270 Views
Kris_Ke
Contributor III

Hi Guille

 

The failure is caused by install wrong SDK.

It is necessary to install SDK RTM 4.0.0, download site below.

https://www.nxp.com/design/software/development-software/s32-sdk/s32-software-development-kit-for-s3...

 

You should be able to config iseled in S32DS3.4 after installed S32K1XX_SDK_4.0.0 and S32K1_ISELED_EAR_4.8.0.exe.

 

Kris

0 Kudos
Reply

5,265 Views
Guille1
Contributor I

Hi Kris,

I am trying to instal the SDK RTM 4.0.0 with this link, but this is what i find "S32 SDK for S321Kxx RTM 4.0.0 as title but with "RTM_4.0.1" to download.

Thanks.

 

0 Kudos
Reply