I2C slave address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C slave address

1,747 次查看
soniyajchand
Contributor II

I need to configure S32K148 board in I2C slave mode. How do I set the slave address of the device or is the slave address already given? I couldn't find it in RM or DS.

 

Regards,

Soniya Chandran

标签 (1)
0 项奖励
回复
1 回复

1,728 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Soniya Chandran,

Please refer the lpi2c_slave_s32k148 in S32SDK S32K1xx RTM v3.0.0 Example Projects.

lpi2c_slave_s32k148.pngLPI2C_Set_SlaveAddr0.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复