How to use S32K144 FlexCan Interrupt to recieve can data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use S32K144 FlexCan Interrupt to recieve can data?

Jump to solution
4,589 Views
victor_song_171
Contributor III

Just like the title.

I want to use FlexCan Interrupt to recieve can data with the S32DS.How could I do? What config and code have to do ?

PS : Just use S32DS IDE and s32k144 SDK,not simulink and IAR.

Labels (1)
1 Solution
4,176 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you are using the SDK, the CAN driver installs and calls interrupts upon each transmit/receive operation, you need not to do any further setup. Just you can install a user callback function which will be called from MB interrupt and you can distinguish between several events.

See more info about interrupts here;https://community.nxp.com/message/1045615 

BR, Petr 

View solution in original post

4 Replies
4,177 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you are using the SDK, the CAN driver installs and calls interrupts upon each transmit/receive operation, you need not to do any further setup. Just you can install a user callback function which will be called from MB interrupt and you can distinguish between several events.

See more info about interrupts here;https://community.nxp.com/message/1045615 

BR, Petr 

4,176 Views
victor_song_171
Contributor III

thank you for the assistance. The issue is done.

0 Kudos
Reply
4,176 Views
victor_song_171
Contributor III

but how could i config the filter for recieved can id ?

0 Kudos
Reply
4,176 Views
PetrS
NXP TechSupport
NXP TechSupport
0 Kudos
Reply