How to use ORTI file in S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use ORTI file in S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0

2,122件の閲覧回数
decoski
Contributor II

Hello,
I use S32K_ AUTOSAR_ OS_ 4_ 0_ 98_ RTM_ 1_ 0_ 0 for sample1 debugging. Using the default sample1. ort file (due to warnings, version 2.2 has been modified to 2.1), the IDE is IAR V8.32.1,Optimization level is low, loading ORTI is normal. However, the ambiguous symbol(@Mark 1 on the diagram) warning is displayed as shown in the figure, and the task priority(@Mark 2 on the diagram) cannot be displayed correctly. It is considered 5 (should be 0---5). How can I solve this problem? Thank you!屏幕截图 2023-07-10 184059.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,045件の閲覧回数
NamLee
NXP Employee
NXP Employee

Hi decoski,

Sorry for this lately reply, the NXP site was down last week and i check your ticket this week.

In the Release note of the AUTOSAR OS package, you can find a note of compiler requirements as below:

NamLe_0-1690354599322.png

You should use the following version of all required tools/enviroments

I'm not so sure about the second issue but maybe it can related to the first one, so please help me to try re-install correct version of tools once again.

Thank you,

Nam.

0 件の賞賛
返信