How can I get the last SDK version for S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I get the last SDK version for S32K144

ソリューションへジャンプ
4,490件の閲覧回数
pengchenbing
Contributor II
Dear support team,
   How and where can I get the last SDK version for S32K144 ?
   And I create a new S32DS projection in DS32 , but none components can I add to it ,I want add FreeRTOS component to it .
   

Regards,

0 件の賞賛
返信
1 解決策
3,399件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Peng,

I'd recommend you to install the latest update (S32 Design Studio for Arm v2.0 - Update 2 available)

It includes the latest S32K14x SDK v0.8.5 EAR - see the release notes attached with the release announcement for more details about features and "What is new".

Regards,

Stan

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,400件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Peng,

I'd recommend you to install the latest update (S32 Design Studio for Arm v2.0 - Update 2 available)

It includes the latest S32K14x SDK v0.8.5 EAR - see the release notes attached with the release announcement for more details about features and "What is new".

Regards,

Stan

0 件の賞賛
返信
3,399件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello, 

On main menu bar click on File -> New S32DS Application project

pastedImage_1.png

Select S32K144 device and put unique project name 

pastedImage_2.png

In next step select S32K144 SDK:

pastedImage_3.png

Double click on processor expert and add FreeRTOS component. Don't forget generate Processor Expert code. 

pastedImage_4.png

Change FPU instructions settings by right click on project name -> properties 

pastedImage_5.png

Other way is use and modify FreeRTOS example.

Jiri 

0 件の賞賛
返信