HELP! "No such file or directory" and "SDK RTM 1.0"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELP! "No such file or directory" and "SDK RTM 1.0"

1,609 Views
wyj122793
Contributor II

Strange problem: I added the eee module to my project through SDK RTM 1.0 and generated it after configuring the SDK.Then I debug the project without doing anything else.

 There is an error:  "Description Resource Path Location Type
eee_driver.h: No such file or directory Cpu.h /TCU_OS/Generated_Code line 64 C/C++ Problem".

But I checked the path and include Settings, and it included the path.More details are shown below.

Q1.pngQ2.pngQ3.pngQ4.png

Labels (1)
2 Replies

1,482 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Please share what do you have in Console Tab. Sometimes the Console output is not synchronized with Problems tab.

Best regards,

Razvan

1,482 Views
wyj122793
Contributor II

Thank you for your reply! I've solved the problem, although I still don't know why it happened. My approach is to re-create a project and then migrate everything from the current project. Then the problem is solved. Maybe my previous project had some irregular operation in path setting, which caused the problem. I'm sorry that I can't provide the content in the console because the previous project has been deleted. Hope my operation can provide some reference.

0 Kudos
Reply